Why miss a decibel of life?
The audiogram below demonstrates conductive hearing loss. In this example, the inner ear works properly but something inhibits sound from getting through the outer/middle ear to the inner ear.
Learn how to read an audiogram
The hearing loss displayed above ranges from 30 to 50 dB HL in the right ear and between 35 and 45 dB in the left ear. This individual would only be able to perceive fragments of normal speech, which has a loudness level of about 65 dB. A normal hearing person has a dynamic range of up to 65 dB between listening threshold (at 0 dB) and speech level (at 65 dB). The person with the described hearing loss only has a dynamic range of about 20 dB. This difference of about 45 dB must be amplified to enable the person to perceive speech and sounds appropriately.
If the inner ear is unimpaired, bone conduction hearing solutions do not deliver any amplification. Their task is only to make sounds audible by an adequate vibration of the skull, which transfers the sound information directly to the inner ear. Starting from there, the hearing process continues normally.